TGML Elliptical Pie: <Pie>

Pie defines an elliptical pie slice. Pie is similar to Arc.

Attribute Type Description

Center

Point

The center point of the ellipse.
Default: "0.0 , 0.0"
Inheritable: No
Animatable: Yes

Fill

Brush

Specifies how the interior of the shape is painted.
Default: "None"
Inheritable: Yes
Animatable: Yes

Opacity

Double

A value between "0.0" (transparent) and "1.0" (opaque)
Default: "1.0"
Inheritable: No
Animatable: Yes

RadiusX

Double

The horizontal radius of the ellipse.
Inheritable: No
Animatable: Yes

RadiusY

Double

The vertical radius of the ellipse.
Inheritable: No
Animatable: Yes

StartAngle

Double

Specifies the angle between the x axis and the starting point of the arc.
Default:"0.0"
Inheritable: No
Animatable: Yes

SweepAngle

Double

Specifies the angle between the starting and ending points of the arc.
Default:"0.0"
Inheritable: No
Animatable: Yes

Stroke

Brush

Describes how the line is painted.
Default:"#000000"
Inheritable: Yes
Animatable: Yes

StrokeDashArray

Array of Double

The pattern of dashes and gaps used to outline shapes:
"<dash> [ <gap> <dash> <gap>...]"
If the array only specifies the first dash, the line is patterned as if a gap with the same length as the dash was specified.
An array with only one dash set to "0" will result in a line without any pattern.
Default: "0"
Inheritable: Yes
Animatable: Yes

StrokeWidth

Double

The width of the outline of a line.
Default: "1"
Inheritable: Yes
Animatable: Yes

Visibility Visibility

Specifies if the element is visible or not.
Default: "Visible"
Inheritable: No
Animatable: Yes